Part Number: PCM2707C Hello,
This component (PCM2707C) with the USB to I2S interface will be soon obsolete. Do you have an alternative / a new reference ?
Thank you & have a good day.
Part Number: PCM2707C Hi Ti Team,
1,Is there any way to change the default name of the PCM2707 chip connected to the computer to the name we need, and solidify it inside the chip (that is, without i2C to control it)
2,The sound card of the computer cannot…
Part Number: PCM2707C Hi Experts,
Good day. Seeking advise on this query:
I want to use PCM2707 to convert usb to i2s. And then, I have to upsampling the i2s signal because the DAC that I want to use only allows 24bit 96kHz signal.
The problem is that…
Part Number: PCM2707C Hello,
I would like to change the USB descriptor data with SPI.
What am i doing wrong here?
First line is CS, than the data and as a third the clock.
Both PSEL and host lines are high. D+ line is pulled low.
Thanks!
Part Number: PCM2707C Hi team,
Every-time you plug in the USB HID device into a computer, the name of the device is USB AUDIO TI and it auto detects correctly. Is it possible to change the name of the device to something else?
Thanks,
Connie
Part Number: PCM2707C In short, I'm looking for a simple OTS USB-to-I2S bridge. I want to interface to a PCM1860 ADC and a PCM5102A DAC and am curious if this part -- the PCM2707C can achieve this.
We planned to use the NRND CP2615 bridge but found…
Part Number: PCM2707C Hello,
Our customer look for the D to D converter device like USB Audio Class 1.0 input to I2S output.
Which aimed to get audio signal from gaming machine such as Nintendo Switch or Playstation.
We expect PCM2706C and PCM2707C are…
Part Number: PCM2707C I´m Trying to desing a USB to I2S bridge using the PCM2707C . As I understand the device should be automatic recognized by windows (10 in my case).
However I always get a error unknow device A request for the USB device descriptor…
Part Number: PCM2707C
Hi, I'm using this device Soprano_DAC.pdf in one of our amplifier and we have some problem of faulty. Sometimes this component, when the customers connecting the USB from PC o Laptop, broken and we have to replace. We check all…
Part Number: PCM2707C I want to use the PCM2707C as a bridge between an I2S codec and USB. The application would be to make a USB microphone / speaker device. I have an eval board from Maxim that uses this part, but so far I have only seen the USB DAC…