Part Number: PCM5121
Hello all,
I am working on a new board that uses an PCM5121, it is connected to an ESP32S3 microcontroller.
Here is the schematic related to the PCM5121:
I would like (but there is no absolute need) to use the PCM as a slave. I…
Part Number: PCM5121 Hello,
I am using PCM5121 and I am providing 24.576MHz to SCK/BCLK with Fs of 192KHz. The LRCK width is one cycle. I have programmed it in TDM/DSP mode. Also, the Auto clock mode is enabled.
The problem is that the Right channel data…
Part Number: PCM5121 Other Parts Discussed in Thread: PCM5142
Hello,
How to configure the 1.1 channel output? During debug,EQ1 and EQ 2 are sync, how to configure them independently, for example EQ1 is used for low-pass filter and EQ2 is used for high…
Part Number: PCM5121 Hi
My customer care about data transmission time of PCM5121. So l would like to know what is t he delay time range of audio data from input to output? Maybe several μs?
Thanks,
Amber Si
Part Number: PCM5121 Hi team,
For hardware master mode, where the BCLK and the LRCLK are supplied by the PCM512x chipset,
How does the PCM512x knows what fs is to clock out by the LRCLK since there are several choices .
For example: when sck is supplied…
Part Number: PCM5121 Hi Team,,
My customer is currently looking at using TI Audio DAC for their project.
They are currently looking at PCM5121. Please see the below enquiry:
Pin 14 can be use to choose between I2S Master or I2S slave, and pin 24 can be…
Part Number: PCM5121 The temperature information of the PCM5121 is a little confusing. Here Information of datasheet:
Here the information of product web site:
Can the PCM5121 be used in an industrial temperature range with an ambient -40..85 °C…
Part Number: PCM5121 Other Parts Discussed in Thread: PUREPATHSTUDIO Hello Experts, My customer is considering to use PCM5121 by a following conditions. 1. Software mode 2. PLL will use 3. SCK does not input. SCK will create from BCK. 4. mini DSP(fixed function…
Part Number: PCM5121 Hi Team,
when I test the PCM5121EVM the delay time is not match with the datasheet descprition.
in datasheet the 0x02 preset flow delay time is 3.5/fs, when fs=48K, but the AP actual test DUT delay time result is 104.3us.
the 0x07…