Part Number: PCM5242 Other Parts Discussed in Thread: OPA1656 Hello TI-Team, We have a problem with the noise at the output of our DSP board. We want to ensure that the noise is not coming from our output circuitry by evaluating the performance of used…
Part Number: PCM5242 Other Parts Discussed in Thread: PCM5102A , PCM5100A Hello
There are two questions about PCM5242. Hope anyone could help.
1. I found that there is a PCM5242 datasheet with 2.1Vrms output https://datasheet.octopart.com/PCM5242RHBT-Texas…
Part Number: PCM5242 Hi team,
I noticed PCM5242 needs an external headphone AMP to drive a headphone.
Is this because the PCM5242's output current not enough to drive a headphone? Can't we just directly connect a headphone?
Thanks,
Jay
Hi Jay,
You may just submit a new request for the proper part number, I see you listed 2 case numbers, is it one for each device?
Best regards, -Ivan Salazar Applications Engineer
Part Number: PCM5242 Other Parts Discussed in Thread: PCM5102A Hello
I found that there are 4 RC values in datasheet and EVM
in datasheet 8.7.1. Many applications require an external low-pass RC filter (470Ω + 1.2nF) to provide sufficient out-of-band…
Part Number: PCM5242 Other Parts Discussed in Thread: PCM1681 , PCM1690 , PCM4104 I'm creating a system that has 40 mono channels of >= 24 bits x ~4-8 KHz. I need some signal processing and DC coupled output so the PCM5242 seems like a good fit. …
Part Number: PCM5242 Hi Team,
We have requirement to connect this DAC IC with IMX8MM.
So we need updated driver file for the same.
Second requirement:
>> We need to disable/enable this DAC whenever we want ... Can you help us here to enable/disable…
Part Number: PCM5242 Other Parts Discussed in Thread: TPA3255 , SRC4392 Hello
Is it possible to use PPC2 without EVM board? I want to design a board with SRC4392 and PCM5242 to drive a TPA3255 amplifier and host controler (may be MSP430 or atmel 328P…