Part Number: PCM9211 Other Parts Discussed in Thread: PCM5242 , , PCM5121
Hi,
We are using PCM9211 for Optical and Coax RCA along with Analog Audio Inputs. Please confirm if we can connect the output from PCM9211 as I2S directly to the Audio DAC like PCM510x…
Part Number: PCM9211 Hi,
We have to process the digital data coming from S/PDIF OR TOSLINK along with a seperate path via Analog Audio as shown in the block diagram shown below.
I am going through PCM9211 datasheet and it looks like it can handle all…
Part Number: PCM9211
Hi,
I understand that the audio signal is input through MPIO_C ports and the S/PDIF-encoded signal generated by the DIT module is available through the MPO0 pin. The DIN setup and hold time isn't mentioned in the PCM9211 data sheet…
Part Number: PCM9211 Hi Team,
My customer have received PCM9211 EVK board for evaluation. Currently there is only 1 script file, do we have any more script file for reference?
Many thanks!
Part Number: PCM9211 Other Parts Discussed in Thread: TAS5806MD Hello IT team,
We're designing audio product with PCM9211.
It has two inputs which are ADC(using VINL/VINR) input and I2S(using AUXIN0).
And it has a I2S output(using MAIN OUTPUT PORT…
Part Number: PCM9211 Hello,
I would like to integrate the AC-MB on a mechanical part so I need a 3D model of the AC-MB to verify there is no interference.
Could I get a .STEP or other format to import the Board in Catia?
Thanks
Part Number: PCM9211
Hi,
Do you have a device to support SPDIF to surrounded sound format 5.1? I think that would need 6 outputs, right? Or we can have external MUX and control it in some way?
Thanks,
Zach
Part Number: PCM9211 Other Parts Discussed in Thread: PCM1794 Hello,
I noticed the following strange behavior:
The signal comes in via RXIN6 and is sent to TXOUT and RECOUT1 in parallel:
Register 34: B11000110
Register 36: B00000110
From the MPO0 output…
Part Number: PCM9211 Hi,
Currently, I'm using PCMDEVICE codec driver for PCM9211. But, I found the function: pcmdevice_regmap_read() always returned error meaning reading pcm9211 registers failed. I debugged the code, but didn't find the solution.…