Part Number: PGA2311 Other Parts Discussed in Thread: PGA2310 Hello,
I am operating PGA2311 under +/-5V analog supply. Since it is presently unavailable in stock for the quantities I need, can I buy PGA2310 in its place? SOIC version. Will work it work…
Part Number: PGA2311 I am trying to incorporate the PGA2311 into a new design. I can see from the data sheet that on start-up all outputs are in the mute condition until a new setting is programmed by the host controller. However, and I'm sure I've seen…
Part Number: PGA2311 Other Parts Discussed in Thread: PGA2310 , , PGA2320 Hi TI experts,
We are looking for volume control IC.
Do you have S/N spec of PGA2310, PGA2311 and PGA2320?
(Test condition : Vol=0dB,Rg=0 Ω, A-weight)
Please check it.
Thank you.
Part Number: PGA2311 Hi Team,
Good day. I am posting this inquiry on behalf of the customer.
" How do I change the dynamic range from -95.5 to +35.5 dB to -40 to +18 dB ?"
Please help to advise. Thank you for extending your support.
Kind regards…
Part Number: PGA2311 Is it advisable to cascade the two halves of the PGA2311?
I have done this on my design and the device shuts down depending on what gain combination I enter.
I do not believe I am reaching the maximum output levels, so not quite sure…
Part Number: PGA2311 Hi team,
Good day. Our customer would like to use two PGA2311, one for the left and and one for right channel. Can the analog inputs and outputs channel can be connected in parallel for the two PGA2311?
Regards, Carlo
Part Number: PGA2311 Other Parts Discussed in Thread: LM2662 , LM828 Hi' All
There was a thread 2 years ago with no solution and I have not been able to find an answer.
I need to run the PGA2311 in a single supply operation for the analog part
So Va…
Part Number: PGA2311 Hello,
Because PGA2311 output stage of analog part is an opamp I would like to know if there is stability or other issue when the output of channel is connected directly to a dc blocking cap ?
My design is based on PGA2311 and just…
Part Number: PGA2311 Hi Team,
PGA2311 has zero-crossing detection function for noise-free level transitions. Does it mean that PGA2311 automatically changes between the specific gain setting with lowest output noise when there is no input signal and the…
Part Number: PGA2311 Other Parts Discussed in Thread: TPS7A49 Hello, I'm designing a high end quality A class amp and would like to use PGA2311 to add digital volume control. My design has separate analog ground for both channel in order to keep a very…