Can I convert the resolver value to analog and use it? AOUT is confirmed on the pin, and the user wants to check whether it can be converted to ADC and used (currently, it is difficult to use serial communication or parallel bus).
Thank you.
Other Parts Discussed in Thread: PGA411-Q1 Hello everyone,
we are using a PGA411-Q1 in our project. We are using the the SPI-Interface of the "resolver chip" to read the rotation speed as well as the serial interface to read the resolver position and…
Part Number: PGA450-Q1 Other Parts Discussed in Thread: PGA411-Q1 Hi,
Is this PGA411 still the main recommendation? Is there a new product in the back? There is no complete alternative, including hardware and software.
Thank you !
Part Number: TIDA-01527 Other Parts Discussed in Thread: PGA411-Q1 Hi All,
Does anybody has PGA411.h & PGA411.c device driver files for PGA411-Q1 resolver to digital converter IC or a link to where they can be downloaded. I found this link http…
Other Parts Discussed in Thread: PGA411-Q1 Hello,
I am using a PGA411-Q1 to measure rotor angle in motor control application. I want to prevent the resolver output from turning off under any condition (even potentially damaging faults) during operation…
I need to drive resolver with follow characteristic :
Resolver Pair Poles = 6 ( means 3 KHz freq on SIN COS signal at 30000 RPM )
EXC Impedance = 50 Ω ( @ 10 KHz)
EXC Voltage required = 7 VRMS
PGA411 Resolution = 12bit
With previous characteristic…
Other Parts Discussed in Thread: PGA411-Q1 Hi there
i'm using pga411-q1 encoder signal OUTA OUTB to calculate speed and angle of motor
something i want to say is how can i get some more information about encoder_emulator in pga411-q1
i read the reference…
Other Parts Discussed in Thread: PGA411-Q1 Hi,
I am considering PGA411-Q1 for use in an automotive application.
Please can you advise me regarding the future availability of this part?
Thanks,
Anthony
Part Number: PGA4311EVM Other Parts Discussed in Thread: PGA411-Q1 , PGA4311 Hi Yanmin Luo Greetings!
we are working on PGA411-Q1 EVM .
The default UI is set to default 4V RMS value, but our configuration required 7V RMS value that we are able to set,
…
Other Parts Discussed in Thread: PGA411-Q1 Hi
We are using PGA411QPAPRQ1 is our design. Our current boards are working well with this
System is not even accepting this part number or simply PGA411-Q1
I have seen threads like e2e.ti.com/.../pga411-q1-al…