Part Number: PGA450Q1EVM Is the "PGA450Q1EVMS_UART_Demo.ino" out yet? I have not been able to find it and I am trying to get this part to work with a MEGA. This is for a self driving RC car. Any help is greatly appreciated.
Thank you
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: TUSS4470 , PGA450-Q1 , PGA460 Hi there!
I am working on a design to detect an approaching object and then to generate an alert when an approaching object is detected.
I am trying to compute the latency…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: PGA460 Hello
Has PGA450 been superseded by PGA460 or are they two different things?
If they are two different things does the PGA450 include the actual ultrasonic sensors?
If sensors are included…
Part Number: PGA450Q1EVM Hello, All
I was testing for long mode of PGA450Q1EVM
The peak echo signal was weak over 2.5m so I tried to change the configuration of VREG, Transducer Freq(0.2 step) and Burst count by one step on tap of Evaluation in GUI
but…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: TIDA-00151 , PGA450-Q1 , Hi!
I do not get the expected response from the PGA450Q1EVM-S (TIDA-00151), purchased April 2019 when interfacing using an Arduino MEGA on Serial1 UART programmed with the…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: PGA450-Q1 , , PGA460 , PGA460-Q1 Hello,
I have a PGA450-Q1 EVM, and connecting the included 58kHz transducer works fine. I would like to switch to the 48kHz transducers from Bosch:
I have removed…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: TIDA-00151 Hello,
I am using PGA450Q1EVM with the TI GER Board and my problem is when I connect (via usb) the TI GER board to my PC, Windows don't recognize the board as Serial COM. But it's still…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: TIDA-00151 , , PGA450-Q1 Hi there, I am working with the PGA450Q1EVM REV-C (including TI GER-A board and Murata transducer). I got familiar with the GUI and I am able to get range profiles from it…
Part Number: PGA450Q1EVM Hello,
I have a question about 11.2 Monitoring the Signal Path of PGA450Q1EVM User's Guide(SLDU007C).
[Q]
(a) DACO pin = TESTO_A ? I have read the following sentences at User's Guide(SLDU007C), p20, 11.2 Monitoring Signal Path…
Part Number: PGA450Q1EVM Other Parts Discussed in Thread: PGA460-Q1 , PGA450-Q1 , MUX36D08 Hello
I wonder that I bought a car rear sensor and inspect into a car rear sensor
there were connected with 4 transducers on a chip so that I want to connecte with…