Part Number: DRV2700EVM-HV500 Other Parts Discussed in Thread: DRV2700 Hi, I'm Jeon Hyeon Min.
I'm using DRV2700EVM-HV500 for driving piezoelectric actuator.
What I want is 0~158V AC sine wave output for 0~200Hz using DRV2700EVM-HV500.
So I found…
Part Number: DRV2700EVM-HV500 I'm running windows 10 and trying to connect to my DRV2700EVM-HV500 but the device is not recognized by piezo control console. When I try to follow the firmware update/scan device procedure the board doesn't show up, I just…
Part Number: DRV2700EVM-HV500 Hello,
I set the waveform as the picture billow using Piezo Control Console . I want this waveform to be output only once when I click "Send Waveform". But the waveform was output 4 times. What caused this to happen…
Hello. Janz,
Thank you for your answer.
I successfully upgraded to Version 1.7 using Piezo Control Console.
However, firmware upgrade still cannot be performed on UniFlash.
Can DRV2700EVM only download firmware from Piezo Control Console?
Regards, Sim…
Part Number: DRV2700EVM Hi all,
I am trying to use PiezoControlConsole.exe to drive DRV2700EVM DRV2700EVM but my laptop cannot recognize DRV2700EVM. From the GUI, the USB button is blank like this:
My laptop system is win10. I tried to update the firmware…
Part Number: DRV2700EVM Hi Ivan,
The customer installed the Piezo Control Console bit it doesn't work with Windows 7 Enterprise Edition. Does it support Windows & Edition?
Regards,
Danilo
Part Number: DRV2700EVM Hello
I started the testing of this module with the delivery configuration, however:
The Piezo Console software detects and recognizes the module, but it crashes when I press "Connect".
I updated the module firmware with…
Hi Sydney,
Thank you very much.
I closed JP13,
I enabled output via the Piezo Console.
And with a multimeter I measured 22V between OUT +/ -.
This gives you a small sign of operation.
However, my Jumpers JP7, JP8, JP9 are
In EN/MSP
GAIN 1/MSP…
Part Number: DRV2700EVM Hi all,
I was trying to test the DRV2700EVM following the procedure on the User Manual.
On the GUI, however, the connect button was grey. I tried on Win 7 and Win 10 but none of them recognized the device.
Could you please help…
Part Number: DRV2700EVM Hi experts:
I'm trying to drive my piezo speaker with DRV2700EVM, but Piezo Control Console crashed when I click console, my PC OS is Win7.
if I use analog input by an external signal, just connect JP7,JP8,JP9 to PU, remove jumppers…