Part Number: PMP10081 Hi,
simulation of the sepic converter using pspice for Ti has been given here.
In this circuit the out put vave form is not correct after 0.5ms the output voltage drop to zero.
vin : 15v
Vout : 14.2
could you please help me to solve…
PMP10081 is a battery charger with a CV and a CC control loop. One divider is used for setting the output voltage, the other divider is used to combine the CC and the CV feedback signal.
Part Number: TLV9102 Other Parts Discussed in Thread: PMP10081 , PMP30104 , TLC272 , , TINA-TI Hi support team,
TLC272 is used in PMP10081 and PMP30104.
www.ti.com/.../PMP10081 www.ti.com/.../PMP30104
Is it possible to use TLV9102 instead of TLC272?
Regards…
Part Number: TPS40210 Other Parts Discussed in Thread: PMP10081 , PMP30104 Hi support team,
I want to trickle charge Ni-Cd battery with SEPIC. Is it possible to realize a constant current circuit with TPS40210?
Vin: 24V Vout: 30V or less Charging current…
Hi EM, Thank you for your support.
I realized that it would be difficult to achieve with the circuit I attached. You introduced PMP10081. Is a similar circuit feasible with TPS55340? It seems that ISNS of TPS40210 realizes constant current. I can't find the…
Part Number: PMP10214 Other Parts Discussed in Thread: BQ24650 , , BQ24450 , LM5176 , PMP10081 Would a PMP10214 work with a BQ24650 or BQ24450 in a 12 volt to 12 volt battery to battery charger?
Part Number: PMP7282 Other Parts Discussed in Thread: LM5116 , , PMP10081 , PMP30168 Hi Sir,
What is the actual purpose for using D2 diode in the circuit, Is it only for efficiency improvement or any other purpose is there?
Will the LM5116 controller start…