Part Number: PMP10195 Other Parts Discussed in Thread: TIDA-00173 ,
Hi,
I'm trying to customize PMP10195 reference design, but I find the startup circuit expensive with the use of the MOSFET Q3: STP3N150. Looking into the reference design TIDA-00173…
Part Number: PMP30495 Other Parts Discussed in Thread: PMP10195 , , PMP12082 , PMP41063 , PMP41031 , PMP10415
Hi,
We need to develop the isolated DC-DC converter. You can see the specifications below. In addition, we need additional at least 5000kV isolation…
Part Number: PMP10195 Other Parts Discussed in Thread: PMP12082 , TIDA-00173 We are in need to develop Isolated DC-DC converter with below specifications
Design-1
1) Supply Range: 100V-1000V DC
2) Output 5V at 1Amp
Design-2
1) Supply Range: 100V-1500V…
Part Number: PMP10195 Other Parts Discussed in Thread: UCC28711 , LM5020 Hi,
I'm using this reference design for a flyback design. My input voltage is 100 to 1200 VDC. I have two questions:
First: I see D1 is 110V. So for the VOR I'm saying:
With…
Part Number: PMP10195 Other Parts Discussed in Thread: UCC28711 , Hello,
PMP10195 reference design claims less than 70-ms startup time. It uses a MOSFET STP3N150 for the startup network, but this FET is expensive. Is there a reference design or approach…
Part Number: LM5020 Other Parts Discussed in Thread: PMP10195 Hi,
I am working on the above mention reference design, but transformer design specs is not available in the technical documents. Can it be shared, so that design can be finalized. Secondly…
Part Number: UCC28711 I have a 3 phase diode rectifier with 47uf capacitor feeding the UCC28711. The DC bulk voltage nominal range is 70vdc - 540vdc. I have a 950V 9A SJ MOSFET. The output is 24vdc at 1A and the bias is 12v. My transformer turns count…
Hi Sheldon,
I would suggest LM5020. PMP10195 would be good to look at: http://www.ti.com/tool/PMP10195
Please note this controller does not have burst mode however.
Best Regards,
Ben Lough