Part Number: PMP11107 Other Parts Discussed in Thread: UCC24612 Hi Team,
How does the Self driven SR circuit in the PMP11107 design behaves in the discontinuous mode of flyback application. I am working on the flyback design and tried to implement and…
Part Number: PMP11107 Other Parts Discussed in Thread: PMP11065 Hi,
in the flyback converter reference designs PMP11107 and PMP11065 the author implemented a self-driven secondary rectifier:
It works reasonably well in situations where one does not…
Part Number: PMP11107 Other Parts Discussed in Thread: TPS23753A Hello,
The reference design PMP11107 is presented as a PoE class 3 application and for an input voltage range from 36V to 57V.
I would like to know if it is possible to supply the circuit…
Other Parts Discussed in Thread: PMP11107 We are implementing a 100Mb 803.3af (13W) PoE PD device, power over two twisted signal pairs and 2 spare pairs. This is feeding from PoE Ethernet cable into a "industry standard" Pulse electronics H2019 PoE transformer…
Hello Mike,
There is something like PMP11107 you could consider.
https://www.ti.com/tool/PMP11107
You will probably need a transformer redesign to get more power out of the 3.3V rail, but magnetic vendors are able to do this.
The LM5701 is a PoE PD…
Other Parts Discussed in Thread: PMP40274 , PMP4468 , PMP11107 , PMP10871 Tool/software: WEBENCH® Design Tools Dear all,
I have a requirement of a DC DC converter with following specification
Input voltage 18V to 36V
Output1= 3.3V/7.5A
Output2= 1.5V/3A
Input…