Hi,
See my answer below:
(a) PMP11282 isn't designed for variable output voltage application (ex: battery charging). TIDA-01494 has constant current control loop and allows 22V-28V output voltage range.
(b) My understanding is INA181 only amplify…
Part Number: PMP11282 Other Parts Discussed in Thread: UCC28063 , TIDA-00776 , UCC28180 TIDA-00776 is touted as a design that is likely to meet the new harmonic current emissions standards (IEC 61000-3-2: 2014) due to it's continuous conduction mode design…
Part Number: PMP11282 I am recreating PMP11282 in maker-friendly format using Kicad. The only parts I am unsure of is L800 and L804. TDK does not disclose the core size or material. I actually took a ruler to my computer monitor (fraught with peril, I…
hello Gareth
My name is Clodoaldo Prado, I am technician in electronics and I live in Brazil in the state of Paraná.
I wonder if it could do the assembly and testing in PMP11282 Rev A project?
I'm dificulades to get inductors and transformers of…
Hello Adam,
Thanks for posting this question.
Do you need 20A continuously/nominally or is that a peak requirement? (This will help clarify which topology is best suited for your power level)
If you're planning to use analog control, the following reference…
Hi Murthy,
sorry that TI don't have new full bridge LLC , but you can refer the reference design as below link, which meet your spec.
https://www.ti.com/tool/PMP11282
Ted
Our PFC boost controllers can be configured to work as a flyback. Below are some reference design examples
1 phase TM
http://www.ti.com/tool/PMP9730
Interleaved TM
http://www.ti.com/tool/PMP10116
http://www.ti.com/tool/PMP11282
We have the following…
Hi,
There is an updated design built on PMP11064 PCB:
www.ti.com/.../PMP11282
The output voltage was adjusted to 24V for better efficiency.
This design is designed without forced air cooling (natural convention). So you don't need to provide additional…