Part Number: PMP12082 Hi:
the partnumber T1 ( RLTI-1168 Transformer, 800 uH) it's a standard component?, I can´t found the datasheet. Are you shure that is from TE Connectivity?
Thanks
Lucas
Part Number: PMP30495 Other Parts Discussed in Thread: PMP10195 , , PMP12082 , PMP41063 , PMP41031 , PMP10415
Hi,
We need to develop the isolated DC-DC converter. You can see the specifications below. In addition, we need additional at least 5000kV isolation…
Part Number: PMP12082 Other Parts Discussed in Thread: UCC28730 , PMP10415 , UCC28700 , UCC28740 , TIDA-00173 , UCC28742 , PMP22144 We are in need to develop Isolated DC-DC converter with below specifications
Design-1
1) Supply Range: 100V-1000V DC
2) Output…
Part Number: PMP12082 Hello,
On one of our products we are looking to utilize the PM12082 and we see that there is a development board design around it.
Can you please confirm if this design will pass the IEC61000-4-2, 4-4 and 4-5 tests?
Those tests…
Hi Gaurang,
The PMP10195 has particular requirements: the most important was to startup very quickly (only few milliseconds) and this is why it´s so complicated in the startup network. Also it´s only 3W, and you need 5W and 10W version.
For…
Part Number: PMP20122 Other Parts Discussed in Thread: PMP12082 , PMP9053 , UCC28C42 , PMP10833 How can i Convert the Same Design into a 3 Phase Input ? Can i add the 3 phase using diodes ? Just like the refference design of your Poly Phase metering design…