Part Number: UCD3138 I cannot seem to locate design files for UCD full bridge LLC application. I got the firmware downloaded.
also, cannot see PMP20289 ref design file name at all! That is perhaps the half-bridge LLC.
Isn't there one for full-bridge LLC…
Hi Robin,
Great! Yes, the high side bias supply would not be able to derived from the flyback transformer. You can follow PMP20289 for example of using 2x LMG3410 as a half bridge configuration. The difference would be connecting the high side drain…
Robin,
The IPS node was for primary current sense for my other LLC reference designs (For example: PMP20289) with TI GaN devices, but it is not being used in PMP20637 design as TI GaN device provides reliable over current protection already. The PMP11432…
PMP21842 is a high switching frequency (nominal 450kHz) LLC resonant converter design that provides 390V to 12V/500W conversion. The use of LMG3410 GaN device allows the converter to switch at such high frequency because the LMG3410 GaN device has no…