Part Number: PMP20367
Dear all,
For the use of UCC24610D, I notice that there are some extra components connected to the VD pin, i.e. Q501, D501, which don't appear in the datasheet of UCC24610D.
I really appreciate it if someone can tell what are…
Part Number: PMP20367 Hi Expert,
I am using the PMP20367 reference design for one of my projects. My questions are:
1. Which heatsink part number is recommended for use with the rectifying diodes(D23,D24,D25 and D26) used in the circuit.
2. Do I need…
Hi Yunsheng,
My application is a 300 W, 24 V converter. Similar to: PMP20367,PMP30192,PMP11237 etc. One of the reason for choosing UCC29950 , is that there are many design examples available on ti site.
If you strongly recommend using ( UCC28180 )+LLC(UCC25640X…
Other Parts Discussed in Thread: TIDA-00200 , PMP10283 , PMP9739 Hi Everyone.
Planning to use TI power supply for our new design. But our main concern is that how can i get the same transformer used in the design (Transformer mentioned in BOM).While searching…
Part Number: UCC256301 Other Parts Discussed in Thread: UCC29950 , Hi Sirs,
we have two 450W and 750W PSU project.
And we do reference TIDA-01501 for 450W project.
could this same chips solution apply to 750W?
or I saw UCC29950 can output 750W in E2E. …
Hello KJ
Yes - the UCC29950 can control a 600W power stage but we don't have a reference design at tha tpower level.. The main thing to do is to make sure that the input current sensing signals are scaled correctly - that is the signals into the PFC_CS…