Part Number: PMP10783 Other Parts Discussed in Thread: PMP20708 Hello,
I want to know if I use the same design for low input voltage ( say 30Volts ).?
Since during low input voltage for getting the same output voltage I assume duty cycle of the converter…
Part Number: PMP21455 Other Parts Discussed in Thread: UCC28881 , , PMP20708 In your reference design PMP21455, UCC28881's Pin 4 (named as output in the datasheet) is fed from an external current source.
Is that correct? Why are you suggesting to use…
Part Number: PMP11287 Other Parts Discussed in Thread: UCC3813-0 , PMP20708 Hi, Everyone
My customer is requesting the following power supply.
Input:
AC: 10.2 to 126.5V 50/60Hz±5% DC: 10.2 to 126.5V
Output
DC 12V (about 70mA) or DC 5V (about…