Part Number: LM5176 Other Parts Discussed in Thread: LM25118 , Hi,
my customer would like to choose a device for USB type C power which meet:
1. input voltage range:up to 24V,nominal input may be 12V or 18V
2. output voltage can be set through FB:…
Part Number: LM5176 I derived a design from the PMP21096 reference design, which is basically just page 3 of the original schematic with the resistive feedback values changed.
For testing, I wired a 2.67k resistor from FB to GND to make the Vout approximately…
Hello,
Yes the inductor will affect the efficiency of the efficiency of the converter. One way to improve efficiency is to find an inductor with a relatively lower dc resistance. MOSFET selection has a large influence on efficiency and should be selected…
Hi Takahiro-san,
Thank you for considering the LM5175-Q1. Yes, you can do this by changing the FB voltage. We have reference designs doing this, like the PMP1096 www.ti.com/.../PMP21096
Which has the same concept by altering the FB voltage. The only…
Hi James,
Thanks for reaching out, please use another connector which I used on PMP21096 , the part number is 632723300011 from Wurth.
Best regards,
Max
Hi Devansh, The TPS25740B is a good choice for a 100W Type C and PD charger application. Rather than PMP40312, I recommend looking at the PMP21096. This is a dual solution but you can design it for a single port design. Each buck boost can handle the…