Part Number: PMP21160 Hi,
I want to know why in this board you use 2 UCC 24612 instead of 1 of UCC24624 (it seem more appropriate solution in this case...)
Tank you
Part Number: PMP21160 Hi,
The report assumes an output voltage of 24V +/- 5%.
Is there any easy way to modify the design to adjust voltage up to 28V even with lower performance?
thanks
Part Number: UCC256304 Other Parts Discussed in Thread: UCC28056 , hello
I am tring to review PMP21160.
Below sentance is from PMP21160 test report.
I don't know which one is correct output power 336W? 240w?
Could you plz tell us correct answer.
The…
Hi Ulrich ,
I am very much thankful to you for reply and sharing the valuable information.
Now we are using UCC28056DBV as per PMP21160 from TI, (Rev B) for 50Hz PFC.
Same thing attached here and same components we are using for 50Hz.
Please let us know…
Hi santhibhusan,
You can use LLC controller UCC25640x for DC-DC stage and for AC-DC stage you can use UCC28056
You can refer the following ref design: PMP21160 reference design | TI.com .
Regards
Manikanta P
Hi Danilo,
unfortunately the PMP30092 reference design cannot provide a load current of 14A for 2 seconds, because the output peak power of 344W is too high but there are a few designs in this power range that have been published on ti.com.:
https://www…
Hi Pradeep,
Thank you! Can you also share the design file of the LLC transformer of PMP5141, PMP21160, PMP22087?
You can contact me at yunjing-wang@ti.com. Thank you!
YJ
Hello Sonal singh,
Thanks for your quick reply.
You suggested design has external auxilary power supply in form of TIDA-01503.....link below..
http://www.ti.com/tool/tida-01503
But we would like to design like PMP21160 link below.
http://www.ti.com/tool…
7) On UCC25640EVM-020 Evaluation Module (SLUUBX3B) Figure 4 page 9, what is the bridge rectifier for (self-discharge)? My design is a typical combination UCC28056 and UCC256404 , so I'm not sure whether that circuit is necessary.
>This circuitry is…