Hi,
I had another thing to ask. Is there source code available for PMP21529 software. On the website, I only see an .exe file for the software. Thanks.
Regards,
Amnish
Part Number: PMP21529 Dear Team,
Do this topology can meet this spec as below?
1. Vin :54V +-5% 2. Vbatt: 30V~54.75Vdc 3. Icharge :25A / Idischarge:25A 4. four chargers in parallel.
If not, do you have another suitable solution?
Many Thanks,
Jimmy
Part Number: PMP21529 I saw a installation file online, is there a user guide for it?
Do i use Fusion digital power studio or CCS?
what connector/adaptor/debugger to go the board?
Thank you.
Part Number: PMP21529 It doesn't have current sensor in series with the inductor, when in constant voltage charging, is there only voltage feed back loop? no average current/peak current loop ?
Part Number: PMP21529
I want to start with PMP21529, and play with the software, does TI have this board to sell? what is the cheapest way to get the board?
Regards,
Shengnan
Part Number: PMP21529 Could you confirm on PCB thickness to be used for tidcf34 board 1.6mm or 1mm?
As per Gerber design file PMP21529A.GM10 It is 1.6mm, where as in PMP21529A.GM12 stack up thickness is mentioned as 1mm.
Part Number: PMP21529 Hi TI
Recently I am doing a 3kW BLDC motor power supply with regenerative braking project with 48V battery then I found out PMP21529.
I wondering if PMP21529 support parallel current sharing features and is suitable for this application…
Part Number: PMP21529
Dear Sir/Madam,
I see in the provided schematic, except Iout1, Iout2 are sensed and provided to the digital controller, there are also signals CBC1, CBC2 and Iout2_sense. May I ask what is the use of CBC1, CBC2 and Iout_sense? …
Part Number: PMP21529 I would like to implement the topology described in this reference board using a 3-phase interleaving approach. I am able to calculate the Boost mode ripple current through the output capacitor using equations found in research papers…
Part Number: PMP21529 Hi,
I'm currently based in Singapore and would like to build this reference design to evaluate a 4-switch converter. I am unable to find a suitable part to replace the auxiliary flyback transformer employed in this design.
The…