Part Number: UCD3138A Other Parts Discussed in Thread: PMP21529 ,
hi,
I'm making 4 switch buck-boost converter using UCD3138A. I did analyze the reference design PMP21529 and I saw that it's hard switching between topologies (buck, boost, buck-boost…
Part Number: UCD3138A Other Parts Discussed in Thread: PMP21529 hi,
I want to use UCD3138A in my new project which is based on 4 Switch Buck-Boost like in demo board PMP21529 . In Fusion Digital Power Studio I can't find any design aid for this topology…
Part Number: UCD3138A Other Parts Discussed in Thread: PMP21529 , UCD3138 hi,
can I use the value from FeCtrlxRegs. EADCVALUE.bit.ABS_VALUE in averaging mode? it seems to be ok, but datasheet says that without SAR I should:
"It is also possible to get absolute…
Other Parts Discussed in Thread: UCD3138 Hello There,
I have CCS v3.3 and CCS v10.4 in my labtop but I notice one of firmware codes of UCD3138 cannot be built in both CCS versions.
The firmware code is downloaded from PMP21529 , and it does not link to UCD3138…
Hi,
For bi-directional DC-DC, please take a look at TIDA-00705 ( http://www.ti.com/tool/TIDA-00705 ) and PMP21529 ( http://www.ti.com/tool/PMP21529 ).
Please let me know if any questions or if this is not what you are looking for.
Regards,
Swami
Kaji,
Thank you for the interest in the LM5108. The LM5108 is suitable for a synchronous boost as long as the IC voltage ratings are within the recommended operating range(s). The power train for a sync boost is virtually the same as a sync buck, the…
I have done the similar work in one of my design PMP21529, I also found it takes about 15us for a success transition. The device needs time to stop existing configuration and reconfigure, there is no way to make it faster. You may need to add more output…
Hi CCS folks,
While I'm downloading CCS v6.2, I run into the error as below.
I attach the error log. Please find it and help for the installation?
6840.ccs_setup_6.2.0.00050_install.log
Thanks,