Hi Chin,
The output voltage could be tuned down using the resistor divider to VSENSE.
However I am surprised your performance is so much different than PMP4440. The transformer and resistor divider are the same. The schottky diode is similar. The main…
Part Number: TPS55010 Other Parts Discussed in Thread: , PMP4440 Hi Sir
How to select transform for 5Vin / 5Vout 0.3A application?
Does EVB used "750311880" can be use? enclosed file is i run webench result. is it ok?
TPS55010_design_1079026_1332_134534852…
Part Number: TPS55010 Other Parts Discussed in Thread: PMP4440 Hi,
I would like to design isolation power with below,
Input voltage:5V
Output voltage: 5V
Output current: 300mA.
It seems that TPS55010 cannot support output current of 300mA.
Could you please…