Part Number: PMP5711 Other Parts Discussed in Thread: UCC2897A , LM5034 Dear TI experts,
Is there any minimum load at output side Requirement for PMP5711?.
Regards
Aneesh
Part Number: PMP5711
Dear TI Experts,
What is the use of Q7 and Q8 totem pole driver stage in PMP5711 ?. UCC2897A already having 2A source and sink capacity.
Regards
Aneesh
Part Number: PMP5711 Dear TI Experts
I have doubt on the self synchronous rectification stage used in the PMP5711.
In one of the TI document ( http://www.ti.com/lit/an/slua535/slua535.pdf ) it has been told that If the input voltage range is wider than…
Hello Alvaro,
these drivers are NOT specialized synchronous controllers, it's a standard FET driver. To control these drivers the opposite transformer winding is used, we call it direct driven synchronous rectification. So if the voltage at the transformer…
Part Number: UCC2897A Other Parts Discussed in Thread: PMP10202 , PMP5711 , PMP9127 This is circuit is a reference design for the UCC2897A. The schematic is below. It is using a VB10150C-M3 to recifiy on the secondary side of the transformer. As drawn…