Part Number: PMP5952 Dear Sir/Madam, We have designed a Power Supply based on your reference design PMP5952. Our design is almost an exact copy of this reference design schematic, with the exception of the USB output controllers, which are not currently…
All,
I was wondering if their were Gerber files available for the PMP5952 or PMP5951. Is their a place that sells these PCB's for testing?
Thanks
Chris
PMP5952 Picture shows D2 being a surface Mount part yet the BOM is a MUR180 and it was added on the board. Can I use the Vishay US1K a D0-214AC package
Other Parts Discussed in Thread: UCC24610 Hello sir,
Please find attached schematic file(PMP5952 EVM file). This schematic circuit converts 230vAC to 5v @5A DC
5V power used for USB type C charging circuit, MCU card, RGB card
While testing we observed…
Other Parts Discussed in Thread: UCC28610 Hi,
We have designed 5V@5A USB charger from reference of below link.
http://www.ti.com/tool/pmp5952#1
First trial: when we start testing of our board, It works fine without load but when we applied 2A load to circuit…
Hyukjun,
sorry for the delay. I took a few days off work recently. Check out these reference designs that are closer to your requirements:
Or you can search your requirements to find other designs here:
Let me know if these are of interest and we…