Hi Mike,
Thanks for the reference guide, it is definitely interesting and helpful to better understand the device.
I read that in PMP6023 reference design guide's introduction.
is 0-10V dimming only used in isolated designs?
Thanks,
Kevin
Part Number: TPS92210 Other Parts Discussed in Thread: PMP6023 I looking for below LED driver condition.
・Input:415V AC/DC
・Vout and Iout:TBD
・Need to 0%~100% dimming control
If there match device, please let me know.
Or, I think that close solution is…
Hi Hardik,
Thanks for your interest in TI. At this power level, you will likely want a flyback. Flyback also works well for wider input voltage ranges such as this. For AC input, you likely want a PFC flyback to better shape the input current to achieve…
You have to figure out what the cause of the 87% power factor is. Is this being run in peak current mode control? Constant On Time control would be used for PFC but peak current mode as the PMP6023 works also. Power factor is above 0.9 for the entire…
If you are planning on using 0-10 volt dimming I would look at PMP6023 as your other post talks about. The PMP6023 does not have a set frequency, it varies depending on dimming level and input voltage. The intent of the TPS92210 is to keep the fundamental…
Other Parts Discussed in Thread: TPS92210 , PMP6023 Dear Sir,
I'm looking for a lighting solution which can use the 0-10V control to drive Vout 48V 1.2A (60W) @AC 90V to 305V.
I found the TPS92210, and it also has a TI design for 25W, 0-10V dimming…
The datasheet explains how the TPS92210 works, Constant On Time control versus Peak Current mode control. PMP6023 also explains how it was configured, peak current mode control, and has 0-10 volt interface.