Jeff,
It is used in topologies that use multiple FETs or pulsed transformers, such as active clamp forward or driven flybacks.
An example is PMP6584
If this post answers your question, please indicate so by marking this thread as resolved. Thank you…
Hello,
The transformer is one of the most important parts of a design that determines the system's performance. 8.5V is a non-standard output voltage for PoE, so you probably won't find many reference designs with it. I'll do my best to layout some options…
Hello,
Although there were a lot of questions here, I feel that this was a stream of conscious, so I will try to answer some core concepts here.
For the record, PMP40514 is an Active Clamp flyback. Most of our flybacks are not active clamps. However, most…
Dear Fernandez,
I think the PMP6584 is most efficiency circuit. It doesn't have any high temperature parts.
Thus, my plan is following. Check it whether it is correct or not, please.
1. TPS23753AEVM-001 circuit should be based.
2. Low efficiency…
You might consider starting with the EVM design but use the transformer from the PMP6584 design as the PMP6584 transformer turns ratio will be more suitable.