Yes, I attach my design file. The unsure parameters are Load step, Max dVout due to load step and Vbias at full load. And I would like to have a reference file , can you provide me the one for the PMP6910? My design is quite close to the PMP6910. Please…
In PMP6910 reference design e documents, following are the queries:- 1) Transformer file is showing two secondaries? Are they in Parallel, because schematic shows two SEC in parallel? 2) If we add the another secondary for 3.3Vdc Output, then will it…
Hello Sathishkumar,
Indeed, you can use LM5023 for a 100W converter, with those specifications.
This link http://www.ti.com/tool/PMP4408 takes you to an older reference design for an off-line 120-W dual-output converter.
Obviously, it is not designed…