Part Number: TPS40210 Other Parts Discussed in Thread: TL431 , PMP Hi,
I would like to design a flyback isolated converter, 19V Input, 48V/0.35A output, by following the demo board PMP7132.
However, the schematics I have are from 2011, with the "Preliminary…
Other Parts Discussed in Thread: PMP Hello,
I made a circuit as reference design PMP7132, with the same components values (including WÜRTH transformer), but it is not working.
The output voltage is around 4 V and when I put a osciloscope probe on…
John,
Just to pull this all together I want to make sure I have this correct:
-Starting with my similar to PMP7132 design
-Increase gain for error amplifier from 3 to 10
-Change Chf/Ccomp/Rcomp to 1k optimized values
Are you then comfortable with the…
Please refer to the following E2E thread which discusses the use of TPS2384 (and TPS23841) in a single port application. PMP5480 which is embedded in the thread shows the configuration of TPS2384 in single port applications (auto mode).
http://e2e.ti…