Part Number: PMP7279 Hello, I would like to use the exact same design as the one in PMP7279 : https://www.ti.com/tool/PMP7279#supportandcommunity Every specifications are fitting in my design unless one on the low level Vin input unfortunately. The reference…
Hi Mohsin,
I think PMP7279 might be a good fit for your application: www.ti.com/.../PMP7279
This is a 18V-57V input, 24V, 3A output isolated flyback based on TPS40210.
Best Regards,
Ben Lough
Part Number: TPS23756 Other Parts Discussed in Thread: PMP , TPS2373-4EVM-758 , , , PMP20551
Team,
I am looking for advises (like TI reference design, app notes) for the below scenario:
POE/POE+ with 16 to 57Vin -> 24VDC / 2A
POE/POE+ with 16 to 57Vin…
That's great. I may use the PMP7279 Reference Design, which uses the sam tranformer to bread board a similar design.
Does TI have a list of custom flyback transformers recomended to use with their reference designs?
The TDK Web Sites doesn't seem…
Hello,
I am designing a flyback converter with an output of 24V @ 3A, just like that in PMP7279. The problem is that I can't find the transformer (DCT24LQ-U0XH004).
Can someone advice me on what to do. I have searched but I couldn't find any transformer…
Hello Bruce,
Unfortunately we do not have any designs at this output voltage and power level. My suggestion would be to use one of our reference designs that are 24V output and then modify it for 2A (instead of 3). This would involve changing the transformer…