Part Number: PMP7763 Hi Team,
The PMP7763 reference design shows that it can operate from 30V-800VDC input supply. The datasheet of the T100 transformer shows that it's turns ratio is 8:1 which translates into 30V/8 = 3.75V output from a 30V input. A customer…
Part Number: PMP7763 Does any body could help about where to find the transformer G094173LF from GCi technologies, or perhaps a replacement for it.
I has been difficult for me to find it on the market.
Kind Regards
Part Number: PMP7763 Hi,
I have some questions regarding the PMP7763 ( http://www.ti.com/tool/PMP7763 ), and I'm wondering if it is suitable for a 600V to 24V regulation.
1) The schematic of the current design uses specific components, but will a copy…
Part Number: LM5022 Hello,
I would like to modify the PMP7763 design to yield approximately 30V @ 1.5A out and I am having a hard time specifying an isolation transformer for this design. I would like to be able to accept up to 800V input on the primary…
Part Number: PMP7763 I have a question according to the schemtatics of the DC/DC converter PMP7763. Does it exist any schematics showing the implemented PCB-design? I assume the physical placement of the components might be of importance to the functionality…
Part Number: PMP7763 Has anyone used this design, and if so, how has it worked? I need to operate at an input voltage up to 3000 Volts. I understand that I'll need a higher voltage MOSFET and transformer.
What other changes are suggested?
Since this…
Part Number: PMP7763 Hi Sir/Madam,
Please help to confirm the value of resistor in the reference design, R115 which is 0.82ohm. Customer raised the concern about the resistance value which can withstand for the high voltage application.
Thanks.