Part Number: LM5026 Hi team!
My customer wants to use reference design PMP7892.
Who knows what the characteristics transformer from PMP7892 has?
PMP7892:
Hi, Darwin.
Thanks for your suggestion. but I experienced the same issue at lower o/p loads (0.6A, 1.2A and 2.4A).
My Recent Findings - I found a similar reference design, PMP7892, that had a 20k resistor connected to the TIME pin of the LM5026. The PMP22075…
Hello Wenhsiang Lin
Unfortunately an Excel calculator is not available for the LM5026.
The PMP7892 reference design is located here:
http://www.ti.com/tool/pmp7892
This is a 9.6V to 60V input and 42W output reference. This can be used as a reference to…
Hi H.Someno,
You can just leave the SYNC pin floating if it is not used.
Unfortunately, there is no LM5026 calculator available for LM5026. You can refer to datasheet section 8.2.2 for detailed design procedure with its corresponding application circuit as…
Hi Faith,
Unfortunately an Excel calculator is not available for the LM5026. You can download reference design from below website page.
24-36V and delivers a 12V output at 2.5A.
http://www.ti.com/tool/PMP11478
and
9.6-60V and delivers a 12V output at…