Part Number: PMP8606 Other Parts Discussed in Thread: UCC39002 , , UCC29002 HI sir
I want to add UCC39002 current shunt and +-Remote Vsense function to PMP8606 How can i achieve it
TKS
TIDRBJ0.PDF
Part Number: PMP8606 Other Parts Discussed in Thread: PMP21495 , Hi Team, Our customer is working their design based on the PMP8606 and they'd like to ask if we have the CAD files available for this reference design? We were able to find the files for …
Part Number: UCC28950 Other Parts Discussed in Thread: PMP8606 Hi Ti team
I am using UCC28950 Phase shifted full bridge for EV charger development
Power=3500W,Vinput =380V DC to 425V DC output is 340V to 450V DC
I am using UCC28950 IC in Primary side…
Hi Roberto,
Thanks i am doing this, let me clarify one thing instead of EA+ pin, can i use EA- pin as followed in the PMP8606
Attached my updated schematic, kindly confirm its functionality please
Part Number: PMP8606 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models
Can some share the TINA-TI design for PMP8606?
As schematic is totally different, I can not use "slum276 and slum277" available at www.ti.com…
Hi Giorgio,
In the kW range normally we recommend our Phase-Shifted Full-Bridge which is the UCC28951 . PMP8606 is a 300-W 750-V which might be a good starting point for a kW design.
Part Number: PMP8606 Is this design is suitable for Automotive environment??
I need Calculations and formulas to tune the Input output values according to my requirement. I did not find any technical documents on this link for this design.
The Input values…
Part Number: PMP8606 Other Parts Discussed in Thread: UCC28951-Q1 , UCC28950 1) Is this design is suitable for Automotive environment??
2) I need Calculations and formulas to tune the Input output values according to my requirement. I did not find any technical…
Part Number: PMP8606 Hi,
It would be great if TI can provide design documentation or related white paper for TI reference design PMP8606. Please check the feasibility.
Regards,
Lakshmi.
Part Number: PMP8606 In the TI reference design PMP8606, the current sense transformer T1 is implemented with coilcraft part CS4100V-01L
I noticed that this part is rated to 24A. however, the input current for this application is significantly lower,…