Part Number: PMP9656 Hello,
If I want to use PMP9656 with the same output power range but with an input range from (24V up to 47V), what would be changed in the design, or it will have no effect?
Thank you.
Part Number: UCC2897A Other Parts Discussed in Thread: PMP9656 , PMP3162 , PMP8380 , UCC27511 Hi TI Partner,
After review 3 reference design for 54V to 12V application, I have some questions need confirm with you.
Q1: What is the function of "D8", I see it…
Hi Brian
Our team is testing as you suggested voltage rating should be increase. will get back to you.
please suggest in PMP9656 how overcurrent resistance set in this design .
Thanks & Regards
Ashish
Part Number: PMP9656 Other Parts Discussed in Thread: UCC2897A Hi Sir,
My customer want to design their AC/DC function by using UCC2897A. In PMP9656, we find R3 parallel with T2. Can we know what's the function about R3? Current sense or? Thanks for your…
Part Number: UCC27517A Other Parts Discussed in Thread: UCC27511 , PMP9656 , , UCC27611 , UCC27511A , PMP7451 , PMP3162 , PMP9720 , UCC27517 , UCC27614 Hi team,
For PMP9656, could we use the UCC27517A to replace the UCC27511?
We saw that UCC27517A is with inventory…
Part Number: PMP9656 Other Parts Discussed in Thread: UCC2897A , UCC24612 Hi team,
Could you help check if PMP9656 could goes up to 300W?
If not, what customer should modify to achieve 300W?
And customer also want to know, could they increase the frequency…
Part Number: PMP9656 Other Parts Discussed in Thread: PMP8861 Hi team,
My customer followed the PMP9656 and successfully built a design for 48V to 12/20A applications. Now they have a new project, hoping to extend the input voltage range to 24V-48V, but…
Hi, Sanghyun,
Do you have to keep the same transformer and snubber cap or you are open to change the power stage?
I am not sure where you read UCC28950 is not efficient when input voltage is low. 48V input is not low. Can you point me the source of your…
Part Number: UCC2897A Other Parts Discussed in Thread: PMP9656 Dear Sir,
My cusotmer would refer PMP9656 to a new project: 54Vin to 12V/250W.
Does TI can converter PMP9656 to a .DSN file share to my customer?
Thanks!
Steven
Part Number: PMP9656 Hi Team,
We followed the ref design and built the board according to the suggested BOM, but the EMI test was failed at conductive mode.
Could you please provide the solutions? Thanks!
Best regards,
Ronnie Lin