Hi Youhao,
thanks for feedback.
The pin 2 was short to ground duriing surge test 6kv is injected.
custoler would like to add 10u to PC249 location to test again. P
If The pin 3 is short to ground as surge test 6kv is injected., culd customer improve surge…
Part Number: TPS53625 Hello,
Customer change PR205 empty, PR208->10K / PR210->2K and increase 470uF cap. The specification of Closest and & Farthest DIMM are over DDR spread sheet 30mV as below. The low frequency transient response should be…