Hi Kiyomasa,
Kiyomasa Imaizumi said: I think the PRU is 333MHz in this ADC sample, is that correct?
Yes, you're correct. The Core clk (Hz) in syscfg refers to the PRU clock frequency.
Regards,
Nitika
Hi,
Vairamani Vellingiri1 said: root@am57xx-evm:/lib/firmware/pru# cat /sys/class/remoteproc/remoteproc1/state offline
The processor is already in Stopped state as reflected by offline , so issuing a 'stop' will return a failure.
Are you using 4.19…
Part Number: AM3358 Hi,
when compiling some code for the PRU of the AM3358, the compiler crashes:
INTERNAL ERROR: optpru experienced a segmentation fault
while processing function main file /tmp/TI0LRs1EyhN
This is caused by a defect in the TI C…
Part Number: PRU-CGT Other Parts Discussed in Thread: BEAGLEBOARD-X15 Hi
In Windows 10 Pro, I'm trying to run the example program for PRU core in Beagleboard-x15. I used the ready image " tisdk-base-image-am57xx-evm.tar.xz " from TI linux SDK "…
Part Number: PRU-CGT Hi Experts,
I am using ti-pru-cgt-2.3.2 on linux pc. I have installed MCU PLUS SDK. When I try to build the pru firmware using the cgt compiler. It builds .out but throws error on using hex utility tool
Building secondary target:…
Other Parts Discussed in Thread: OMAP-L138 , PRU-CGT Hi All!
I have attached a minimal working bug in a code composer project.
Environment is the following:
OMAP-L138
pru-cgt v2.3.3
optimization setting: -O0 or higher
The source code is the following: …
Part Number: PRU-CGT Other Parts Discussed in Thread: AM5726 Tool/software: TI C/C++ Compiler Hello
Where can I find a document with all instructions and binary commands representation for PRU-ICSS cores?
As I saw, the document https://www.ti.com/lit/ug…
Part Number: PRU-CGT Tool/software: TI C/C++ Compiler Hello,
I have been trying to understand how to use the hexpru tool to generate an array using the --array option for the utility.
I am getting the following error when trying to use the page0_type_size…
Part Number: PROCESSOR-SDK-AM335X I am trying to run the PRU_RPMsg_Echo_Interrupt0 on a Beaglebone Black on Kirkstone Yocto build. This doesn't run. I get the following, when trying to boot the firmware:
$ echo start > /sys/class/remoteproc/remoteproc0…