Part Number: REF3312 Hello,
I am using REF3312 in current source configuration, connecting a resistor between OUT&GND pins (using GND pin floating). I have configured the scheme as follows:
- Rbetween OUT&GND=249ohm --> Iout=5mA
- Vin to +…
Part Number: REF3312 Hi Team,
we'd like to get 0.5V first using REF3312 and REF35125, then get 0.45V from 0.5V.
I see there is below circuit in REF3312 datasheet to get a voltage from OUT of REF3312 but no guide on range of R6 and R7. Is there requirement…
Part Number: REF3312 Other Parts Discussed in Thread: REF70 Hello,
I am interested in a Precision and Stable voltage reference that could be used as a calibration source in college instrumentation lab. The accuracy value is less critical than stability…
Part Number: REF3312 Hi,
Is there a problem using a higher output capacitance?
In customer design, they used a capacitance output higher than the recommended max value. According to them, even they increase the capacitance to 75uF, it works without oscillation…
Hello,
We do not have a spice model available for REF3112. What stability conditions do you need to confirm?
You could also consider a newer option like REF35125 for your design. It has improved temperature drift, quiescent current, and noise. Its PSpice…
Part Number: REF3312 Other Parts Discussed in Thread: REF2025 Hello team,
I'm looking for a precise voltage reference which has performances below. - Output: 1.2V or 1.25V - Accuracy: <0.2% - Temp drift: <7ppm/C - Drive capability: 10mA< sink&so…
Part Number: REF3312 Other Parts Discussed in Thread: REF3330 , REF3325 Hi,
I checked that REF3312 has SOT-23-3, SC70-3, UQFN package on data sheet and web-site.
But, there is no thermal information of UQFN package.
Could you please check and give me …
Part Number: REF3312 Hello,
How do you measure the voltage reference output to produce a smooth plot of the output voltage vs temperature. There does not appear to be noise in the plot. I would like to reproduce the datasheet's output voltage vs temperature…