Part Number: REF3330 Hi :
Is there any formula of dropout voltage of REF3330AIRSER can provide to me?
Current consumption of my device is typical 0.3305mA or max. 0.44mA and measurement Vout (mean) is 2.9945297V.
I want to check is it meet with spec. or…
Part Number: REF3330 Dear Sir/Madam,
We need your help on a component, REF3330DBZ that we are using in one of our products.
In the attached picture below, you can see that because of the 5V pull-up resistor before the inverter, current tries to flow towards…
Unfortunately this is not available for REF3130AIDBZ.
The closest alternative with model would be:
https://www.ti.com/product/REF3330?keyMatch=REF3330&tisearch=search-everything&usecase=GPN-ALT#design-tools-simulation
Part Number: REF3330 Hello,
I'm writing to ask about operation of the REF3330 when in dropout.
Specifically here are my conditions:
VIN = 3.3V +/-5%
VOUT = 3.0V
IOUT = 4mA (max)
My questions are such:
1. Is the output voltage stable? Will the device…
Part Number: REF3330 Other Parts Discussed in Thread: TMP103 , Hi Team,
My customer is mis-using the device as low Iq voltage source. They don't want to add a new device at this late stage in the design.
How is the current limited and to what level…
Part Number: ADS8866 Other Parts Discussed in Thread: REF35 , , OPA333 , REF3330 Hi -
I am designing with the ADS8866 for a low power application. The TI REF35 looks like it would be the lowest power voltage reference to use.
I noticed in the ADS8866 the…
Part Number: OPA2333 Other Parts Discussed in Thread: REF3330 , SN74LVC2G240 , TPS7A16 , TIDA-00167 Team,
Follow up questions on High-Performance 16-bit PWM to 4- to 20-mA DAC for Field Transmitters article http://www.ti.com/lit/an/sboa379/sboa379.pdf :
What…
Part Number: REF3030 Other Parts Discussed in Thread: REF3330 , REF3033 , REF3025
Hi team,
Could you share below information? We are considering whether REF3030 can be used in the system. One big concern is the dropout voltage. In order to estimate the…