Part Number: REF5030 My customer is requesting a datasheet for an older revision of REF5030. Currently, Rev. K is available on TI.com, but my customer is requesting Rev.J. Could you please send me the Rev.J datasheets?
Part Number: REF5030 I am looking at the Long-Term Stability of the REF7030QFKHT LCCC package. Section 7.11 has a graph, does the stability level out or does it keep dropping over time. Is the long term stability 0 to 1000h @ 35DegC 35ppm while its ON…
Part Number: REF5030 When the material arrived, our quality inspector said the pin was dirty and had secondary tinning. Please help to confirm whether this material has been packed twice, or what is the situation
Part Number: REF5030
Ver.I Y-axis 1mA/div, Iload=-1~+1mA(Read from waveform),
Ver.K Y-axis 1mA/div, Iload=-1~+3mA(Read from waveform),
Different test condition, false record in Ver.K?
Ver.I Y-axis 10mA.div, Iload=-10~+15mA(Read from waveform)
Ver.K Y-axis…
Part Number: REF5030REF5030IDGKR
Without a TI label, is there any way to identify the date code from a voltage ref device? I received a part with top body marked as "TI02" - 1st row and "R50C" - 2nd row and bottom body marked as "02H" - 1st row and…
Part Number: REF5030 Hi,
When I want to simulale the circuit in PSpice for TI with the voltage is Vdc, the result is correct.
I want to see the process of power on, so I replace the voltage source with Vpulse.
When I change the voltage source, the result…
Part Number: REF5030 Other Parts Discussed in Thread: OPA4350 Hi,
Let me ask you a question about low pass RC filter.
I am using REF5030 as a 3.0V reference for ADC.
The configuration of the circuit is following.
REF5030 - RC filter(1K/1uF) - OPA4350…
Part Number: REF5030 Hi Team,
We use REF5030IDGKT part on our board, but it is OOS for some time. Are there any alternative parts to REF5030IDGKT that are available and in-stock? Would need to be pin-to-pin compatible and similar functionality / performance…