Part Number: REF6025 Hi,
I'm looking to use the REF6025 and was looking at the SS pin to maximize the current.
On the pin configuration and functions section it says "Connect to Vin pin for highest current limit", is this a short connecting SS to…
Part Number: REF6025 Hello,
Our customer has a question for REF60xx. There is Figure 17 and 18 (see below) for load transient response in the datasheet(SBOS708B). What is C_L value for these graphs?
Regards,
Oba
Hi YC,
Here are my notes on your REF6025 portion of the schematic:
1. You seem to have a 5 MOhm (mega-ohm) resistor in series with the output capacitor. This is too large. In the REF6025 datasheet there is a 5 mOhm (mili-ohm) resistor. This series resistor…
Hello ttd,
The capacitor characteristics as well as PCB trace length can affect the ESR of a capacitor. Therefore, in some instances, a discrete resistor may not be necessary. Please refer to section 9.3.4 of the REF60xx datasheet for more guidelines…
Part Number: ADS1256 Other Parts Discussed in Thread: OPA350 , REF5025 , REF6025 , REF5050 , , REF6050 , TPS7A87
Here's my 2.5V VREF and 5.0V AVDD circuit base on other post ,
but I am not sure how to define these passive components. Any comments?
Part Number: REF6025 Other Parts Discussed in Thread: ADS1259 Hi,
I apologize that this topic is not related with the REF6025 directly.
Please move to proper forum if this forum is inappropriate.
I watched the delta sigma-voltage reference training video…
Part Number: REF6025 Other Parts Discussed in Thread: REF5020
Dear Sir, please answer
I asked a question about REF6025 in Jun 2017. Please see my circuit in attach.
I need to adjust frequency of generator - 16,384,000 Hz. I need to vary voltage in the…
Schematic_ADC_V0.2.1.pdf
I changed my schematic with the help of your comments:
I removed the 32kHz crystal oscillator and replaced it with a external 16MHz clock oscillator.
I placed the GPIO pins to the GND. I connected a 10k resistor so if i accidently…
Part Number: REF6025 Hi,
three questions regarding REF60xx:
1) Does the yellow marked text refer to CFILT or to CL? (Can the ESR of CFILT really have a noteable impact on the stability as it isn’t a conventional OP/buffer)
2) What is the value of…
Part Number: REF6025 Dear Sir, please, answer
I'd like to use REF6025 for voltage control of Voltage Control Oscillator JT53LV (16 MHz) . Oscillator has control input for feed 1.5 V+/- 1V voltage. I want to adjust this voltage with a potentiometer…