Part Number: REF6041 Other Parts Discussed in Thread: ADS7066 , , ADS7067 Hi, I am considering a topology of a single REF6041 providing reference to up to three ADS7066/ADS7067 ADCs. My goal is to eliminate any headache around designing a reference buffer…
Part Number: REF6041 Hi experts!
Our development team is having a discussion on the discrete components used with the subject part.
This all surrounds the specification of the bypass caps on the reference output. Some of the engineers are requesting that…
Part Number: REF6041 Other Parts Discussed in Thread: ADS8881 , REF70 , REF54 , TINA-TI
Hi,
I'm considering using REF6041 to replace my VREF + OP combination, 'cause the built-in buffer of the former. From the 'Load Regulation' specification I calculated…
Part Number: ADS1258 Other Parts Discussed in Thread: REF6041 , Hi,
In the datasheet it is mentioned that when exiting SLEEP mode there is a small current consumption from the VREFP/N inputs. since I am using LM4040-4.1V for the reference with required…
Part Number: REF6041 Hi
my question is about the opamp that we use it for buffering ADC voltage reference
when reference voltage ICs output is a DC voltage, why we should use wide bandwidth op-amp in case we want to buffer it
what is the roll …
Hello,
The REF60xx or REF50xx families have great devices that should be able to support 24 bit performance. you would be looking at the REF6041 or the REF5040
I also did a quick parametric search for series references and limited the accuracy to 0.5%…
Dear Keith,
Continuation of my previous email.
According to his datasheet, the short-circuit current limit (ISC) of the REF60xx family of devices is adjusted by connecting a resistor (RSS) on the SS pin. The short-circuit current limit when the REF60xx…
Hi Hirotaka-san,
1) DVDD, AVDD and VREF are independent nodes in ADS8864. Your configuration will work fine. 2) The analog core of the device is powered by AVDD.
Which reference driver are you planning to use with this device? We recommend using REF60…