Part Number: BQ79606A-EXAMPLE-CODE Other Parts Discussed in Thread: TMS320F28379D The doubt i have is that the BQ79606 EVM has code support using the TMS570 controller as the host device....and this controller has been used for the UART transmission with…
Part Number: MSPM0L1306 Dear Champs,
I am asking this for our customer.
The user is looking for PMBus 1.2 target example codes, but does not find it in
C:\ti\mspm0_sdk_1_30_00_03\examples\nortos\LP_MSPM0L1306\pmbus
Do we have it?
If not, when will we…
Part Number: IWR6843AOPEVM Other Parts Discussed in Thread: IWR6843 , IWRL6432 Hi TI,
While I compare the resources between IWR6843 and IWRL6432, I am not sure these features for IWR6843 resources are available:
Presence Detection
IWR6843
Have not found…
Part Number: LP5810 Other Parts Discussed in Thread: MSPM0L1306 I am also interested in an I2C implementation using the LP5810. I can not seem to figure out how to use the drive linked in the related question.
Could I get some help in figuring out how…
Part Number: IWRL6432 Other Parts Discussed in Thread: IWR6843
Hi TI folks,
I am new to Texas Instrument development environment.
I did go through the provided user guide : mmWave Demo User Guide (ti.com) and Getting Started With xWRL6432 and knew tha…
Hi Parth,
Thanks for your response.
This is not a standalone application running in DSP1. We are running RT-Linux in A15_0 and TI RTOS in DSP1. Now, we are using GPIO8 exclusively for A15_0 and GPIO2 exclusively for DSP1 to avoid clash between RT-Linux…
Part Number: TMS320F280039 Other Parts Discussed in Thread: C2000WARE Dear C2000 expert,
Currently I'm just trying to build cla example project from C2000ware, but it fails, please look at below errors, can you please help me how to reslove this?
…
Hello Marie H,
If you're having trouble capturing the connection on the sniffer log, it can help to modify advertising to only use one channel, and then make sure the sniffer is sniffing on the same channel. -
Does this means that i need to configure…
Other Parts Discussed in Thread: LP8764-Q1 Hi Expert,
PN: LP876411B4RQKRQ1
As slvaf93a - Scalable PMIC NVM Update Guide mentioned, if the data value of Page 0 register 0x82, ENABLE_DRV_STAT, is not 0x08, then the register CRC for Page 0 and Page 4 must…