Part Number: RF430CL331H Hi, I would like to know if the I2C_SIGNAL pin is helpful in any way. So far the TI code examples of RF430CL331H dont use the pin. Please provide a use-case for this pin or let me know if it's safe to leave it floating.
Thanks…
Part Number: RF430CL331H Hi Team,
Where do I connect the thermal pad of the RF430CL331HIRGTR?
The customer wants to know where to connect thermal pad of the RF430CL331HIRGTR. Where is the recommended connection?
I understand the package thermal pad must…
Part Number: RF430CL331H
Hi Sir,
I would like to ask if the ndef file defines several ID files. Can Android mobile terminal read the contents of the file by reading the ID number?
If multiple ndef files are defined, when I read CC files, I can only…
Part Number: RF430CL331H In the test of using rf430cl331h chip, we found that only 249 bytes can be transmitted. The chip manual says that 3K bytes can be transmitted. What should I do if I want to transmit more than 250 bytes?
Moreover, the application…
Part Number: RF430CL331H Hello,Our company is using RF430CL331 ic, If when make 5 files.such as FileText_E104[100],FileTextE105[200],FileTextE106[300],FileTextE107[400],FileTextE108[500].
When the NFC reader close to RF430cl331, How the RF430CL331 send…
Part Number: RF430CL331H Other Parts Discussed in Thread: TIDM-BIOSIGNMONITOR Hi Team
Hello,I define 0xE104,0xE105,0xE107,0xE108 files in the CC feil such as“www.ti.com.cn/.../TIDM-BIOSIGNMONITOR”modle。 But when I use my phone read the RF430CL331, my phone…
Part Number: RF430CL331H Hi Team,
There is VANT_peak Antenna input voltage specification (Max 3.6V) at 4.4 Recommended Operating Conditions, Resonant Circuit in the datasheet.
How to control / adjust Antenna input voltage?
Is there any guide line for…
Part Number: RF430CL331H Other Parts Discussed in Thread: TRF7970A Hi Team,
Would you please explain the definition for VLIM : Limiter clamping voltage and ILIM,MAX Maximum limiter current in the datasheet as below?
Thanks and Best regards,
Kuerbis. …
Part Number: RF430CL331H Customer tries to bring up his design with CL331H and MSP 430FR2476.
SW is being ported from our ref design with adapting I/Os, clocks and baudrates.
Cmds according erratum are executed at startup.
During communication customer…
Part Number: RF430CL331H Other Parts Discussed in Thread: MSP430FR2475 I implemented an NDEF Type 4 Tag with RF430CL331H by using the communication stack provided in theRF430CL331H_Host_Firmware (sloc330.zip).
The RF430CL331H is connected to a MSP430FR2475…