Hi Samantha Schadwinkel ,
So, it could be due to having multiple EEPS.
I will note this issue for future correction, is it possible for your application to use single EEP with two virtual sectors like as most of the customers use case.
-- Thanks & regards…
Hi Chunyan,
Chunyan Li said: However, around 25 CPU clock cycles seem excessive. Is this level of delay typical for this processor? Are there any tricks to make it faster?
I tested on other Hercules device(TMS570LC4357) and the delay looks same. And a…
Part Number: RM44L920 Other Parts Discussed in Thread: HALCOGEN Hello,
I'm using RM44L920 (100 Pin package) microcontroller in one of my projects. I am facing difficulty and I need help in the following things
1) I am not able to control the state…
Part Number: RM44L920 Other Parts Discussed in Thread: HALCOGEN I am usin RM44L920 eCAP module to measure wheel speed using all 4 eCAP event interrupt and found that during the testing in middle there were speed data and other peripherals are working…
KARTHIK R said: 1)Do i need to increase the VIM channel priority for eCAP interrupts and moving them to FIQ since i am using two ecap interrupt,both ecap interrupt will be happening at the same time(eCAP4 & eCAP6).
You don't have to. The eCAP4 interrupt…
Part Number: RM44L920 Other Parts Discussed in Thread: HALCOGEN Hello,
I've been trying to interface the RM44L920 based custom board with ICM20689 using the SPI protocol. I've understood that for using mibSPI, the master should have a way to let the slave…
Part Number: RM44L920 I am using DCAN1 for sending and DCAN2 for receiving , i checked with logic analyzer that both signals are sent and received but the CAN receive doesn't gets into ISR while data is incoming into the Pins.Can anyone explain me y the…
Part Number: RM44L920 Other Parts Discussed in Thread: HALCOGEN I am using CAN module with external loop back method , but i need to implement in full duplex communication in order to do so i found that sending and receiving side both need to send and…
Part Number: TMS570LS0914 Other Parts Discussed in Thread: RM44L520 , RM44L920 Hi Team,
Due to current procurement challenges our customer is looking for an alternative for TMS570LS0914. They checked that RM44L920 and RM44L520 looks like pin-to-pin compatible…