Hi steven,
thanks for your input.
1. What input voltage will be used? Is OVP not required (input FET is not blocking input adapter OVP)? What is the current limit for the input?
-> The input is connected to the adapter (5.0V/4A) through the eFUSE…
Other Parts Discussed in Thread: TPS61165 Hi Team,
I need to drive the backlight LEDs for 3 different LCD screens. The three different screens have the following configurations:
My input voltage is 12V.
Ideally, I would like to have one SEPIC…
Other Parts Discussed in Thread: DS125BR401A , DS125BR401 Dear Sir,
Gigabyte using DS125BR401A and measure the PCIe Tx signal quality after follow datasheet tuning guide, but the PCIe Tx eye still not improve.
PCIe Gen3 register setting at below…
Hi Anil,
Please take a look at the attached TRM (spruhm8g.pdf). You will find the answer in section 2.2.1 Device Identification. Let us know if you need further assistance.
Cheers!
Krishna
dual_core_delfino_spruhm8g.pdf
Part Number: AM5728
Dear Champs,
In my customer's custom board, they found below SGXInit fail, and they are using Linux PSDK3.1.0.
Could you please check attached log?
Fullscreen
1881.log.txt
Download
�
U-Boot SPL 2015.07-00001…
Addendum (3):
-----Long message due to pasted text....
On a related thread, Ki-Soo Lee on April 2, 2018 (at 6:55am) in response to a similar
question from Jam Cumps, wrote:
>> Thank you. Your file looks fine. Can you provide your configuration…
Hi RonB,
Reply:
1. So, you have moved beyond your problem with fdisk illustrated above?
yes, I already fixed it.
2. Can you provide as an attachment a full log of the new flashing procedure where you write the eMMC?
Insert the log file:
Flash_emmc_process…
Hi,
Yes i did... Here's the .config file having all my choices:
Fullscreen
4382.config.txt
Download
#
# Automatically generated file; DO NOT EDIT.
# Linux/arm 3.3.0 Kernel Configuration
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION…
Other Parts Discussed in Thread: ADS1292R hi
iam working with ads1292r chip inorder to acquire respiratory waves using ECG electrod es. Iam having confusion RESPIRATORY IMPEDANCE PNEUMOGRAPHY method measures change in impedance during breathing ...…