Part Number: SIMPLELINK-MSP432-SDK Hi,
In the HTTP server example provided in network services sample programs, DHCP is used to assign IP. Is there any reference on how to assign static IP?
Part Number: SIMPLELINK-MSP432-SDK Other Parts Discussed in Thread: MSP432E401Y Hi,
We are running a HTTP server on MSP432E401Y microcontroller. Can we have persistent connection established with a client?
Part Number: SIMPLELINK-MSP432-SDK Hi,
I am teaching an introductory programming course using some MSP-EXP432P4111 LaunchPads, which we received a few years ago through the TI University Program. These are now considered obsolete, but we haven't had a…
Part Number: SIMPLELINK-MSP432-SDK Other Parts Discussed in Thread: MSP432E401Y Hi,
We are building a product based on MSP432E401Y. The SDK has an example with HTTP server running on a specified port.
Can we also run a HTTP client service concurrently?
…
Part Number: SIMPLELINK-MSP432-SDK Other Parts Discussed in Thread: MSP432E401Y Hi,
We are building a product based on MSP432E401Y. The SDK has an example with HTTP server running on a specified port.
Can we run two HTTP server concurrently on different…
Part Number: SIMPLELINK-MSP432-SDK /* DriverLib Includes */ #include <ti/devices/msp432p4xx/driverlib/driverlib.h>
/* Standard Includes */ #include <stdint.h> #include <stdbool.h>
//![Simple GPIO Config] int main(void) {
volatile…
Part Number: SIMPLELINK-MSP432-SDK **** Build of configuration Debug for project gpio_toggle_output_MSP_EXP432P401R_nortos_ccs ****
"C:\\ti\\ccs1250\\ccs\\utils\\bin\\gmake" -k -j 8 all -O gmake[1]: 'gpio_toggle_output_MSP_EXP432P401R_nortos_ccs…
Part Number: SIMPLELINK-MSP432-SDK
Dear all,
We are creating a new product using MSP432P401R with I2C connection.
I created the project with CCS and check the sample code from TI.
It can transmit I2C data successfully but error after receive I2C data…
Part Number: SIMPLELINK-MSP432-SDK Hi,
I need some help getting mbedtls from the SDK to build using GCC. I have this batch script. Setting it up for the TI compiler works.
Here's the error
Regards,
-Mike
Part Number: SIMPLELINK-MSP432-SDK Hi
I was hoping someone could answer my question regarding the TI Code Composer Studio and MPS432-SDK software
The software is added to our lab image where students are using the MSP432 board.
I believe i installed…