Part Number: AM623 Other Parts Discussed in Thread: SYSCONFIG Dear TI support,
I have question to DDR config for Sitara (AM62). I’d like to know what “Operating Temperature Range” does. I believe it should set dual refresh but if I set -40C to +95C then…
Hello Pratap,
if a call is not possible, what should be the next step to be done to analyze the issue?
For testing purposes Novica configured the WKUP_UART at the beginning in main() of the flashwriter application to check if main() is started, but there…
Part Number: SYSCONFIG Hello,
I have a problem to load a existing config file from my colleague using the SysConfig tool.
Here the failure message that I get:
I do not understand this message. The mentioned Version is already installed on my PC.
Why…
Part Number: TPS65994AD Hi-
We are using TPS65994AD with Intel Tiger Lake CPU to develop the computer for US Army.
I was able to connect a USB-C thumb drive to the system. However, when I connect the Portable SSD such as
https://www.amazon.com/SanDisk…
Part Number: AM2634-Q1 Other Parts Discussed in Thread: TMS570LC4357 Hello Team,
On checking the TMS570LC4357 RM we could notice that the controller supported DMM /RTP interface for debugging. However, this in not seen in the Sitara platform.
Could you…
Part Number: TPS6598X-CONFIG Hi,
please could you check and fix the link.
If I try to download the software:
TPS6598X-CONFIG — TPS6598x configuration tool
I got the message:
The page you are looking for might have been removed…
Hello,
i have a question regarding the correct entry of timings in the sys config tool:
In the JEDEC LPDDR4 standards, many timings are defined as max out of two values, for example:
tRPab min is max(21ns,4nCK)
I have to enter both values in the sys config…
Part Number: AM625 Other Parts Discussed in Thread: SYSCONFIG Hi experts
Do we have a XLS file for configuring DDRSS registers like TDA4 and AM335x EMIF tools? I want to know how the register values are converted according to the DDR parameters and what are…