Part Number: SM73201-ARC-EV Hello I am using RD195 board for Arc fault evaluation I found the schematic and board data files, shared schematic is in .pdf format generated from Alitum. Can the altium schematic file be made available, It will save me a…
Part Number: SM73201-ARC-EV I have 2 issues for my using of SM73201_ARC-EV.
First, 6V(7.1V by measured) DC power supply positive to +6V pin of J8 (J8p1) and negative to GND pin of J8 (J8p2). RS232 interface for TX,RX and GND is connected to J14 and b…
Part Number: SM73201 Tool/software: WEBENCH® Design Tools Hi. My client has a need to develop a DC arc detection system for 24 VDC power distribution lines.
We are looking for something like the: SM73201-Arc-Eval Photo-voltaic arc detection system, but…
Part Number: SM73201-ARC-EV
Hello,
I am using RD-195 Arc Fault detection Development. My built configuration is TM320F28033 / 64 pins package. The only change in the code is in the linker file
where I added FLASHA and FLASHC_1 in the end.
.text :>> FLASHE_1…
Part Number: SM73201 Hi
I am trying to get the RD-195 board built from the available reference design. But I couldn't find the software or GUI for this. Can you provide the software and GUI.
thanks
Aniruddha
Part Number: SM73201-ARC-EV Hello I am using TI-ARC Fault solution as a reference design to build final solution on the top of it. Currently, we are in initial testing of the solution for in house safety compliance.
As per the Firmware file, it includes…
Part Number: SM73201-ARC-EV Hi,
End-customer found 6 units of the 160 units were fails in the PV field site during arc self testing. Two of the 6 units were sent back to DELTA Tainan. After analysis, ,Engineer found the problem on the Q1 transistor (Self…
Part Number: SM73201-ARC-EV Dear Sir or madam, AN-2154 RD-195 DC Arc Detection Evaluation Board includes a TMS320F28033 micro-controller and it was designed in 2012. Is there any hardwares updated on this product (For example, more powerful and higher bandwidth…