Part Number: SMALL-AMP-DIP-EVM Hi
Can you please provide the CE/EU Declaration of Conformity for SMALL-AMP-DIP-EVM?
This product appears to bear the CE-Marking but the EU D eclaration of Conformity is not available on the website.
Thank you
Part Number: SOT23-UNIV-AMP-EVM Other Parts Discussed in Thread: LMV321-N I am confused about the frequency for the PWM signal coming in. It is between 0 and 3.3 V. The C1 and R1 form a low pass filter. Which I calculated to be 33 Hz, so I thought I''l…
Part Number: DIP-ADAPTER-EVM We are planning to use your evaluation board to validate a new fabrication process.
Is it possible to get access to the Gerber for the pastemask top layer?
We could work with any part of the layout file that shows the top…
Other Parts Discussed in Thread: OPA2344 , TLV9002 , TLV2432A , TLV2262A , TLV9102 , OPA2990 , TLV9062 could you help choose a dual op amp with low offset voltage, small IB and small IQ suitable for smoke detectors. Specific requirements are as follows:
Dual…
Other Parts Discussed in Thread: DLPC3470 We used to utilize LC3000 EVM for our structured light application. It fit our requirements of small form factor, low luminosity (~20lm), ability to store patterns for projection and trigger ability. Any suggestions…
Hi Praveen,
Could you share with me which Processor SDK Linux version is being used, and also share the output from dmesg? For example, piping the output from dmesg to a text file and sharing it will be great "dmesg > dmesg_output.txt".
…
Hey David,
Have you looked at the OPA1656? This is one of our modern Burr Brown devices that has ultra low noise and has great THD specifications. It does not come in the dip package however we do have coupon board that converts into pins that can be…
Other Parts Discussed in Thread: OPA189 , OPA388 , OPA187 , OPA392 , OPA376 , OPA191 , OPA192 Thank you for your support.
I'm looking for an operational amplifier for input offset voltage is few micro voltage (for example, 5 to 10 micro voltage).. We are…