Hi Sean,
Thank you for your reply, it is very insightful.
I am not sure that I understood the point made about the small transformer and a push pull driver with the SN6501. Point 3 is understood, no need for those components circled in blue colour…
Hi Artronifs,
Welcome to TI E2E forum and thank you for showing interest in ISO3086T.
Device ISO3086T has an integrated push-pull transformer driver that is based on SN6501 and hence you can equally refer to SN6501 for more information related to…
Part Number: ISO1640 Other Parts Discussed in Thread: SN6501 , SN6505B Hello experts,
We want to use the ISO1640 I2C isolator in our design. The system is having the two ground references GND1 and GND2 and single power supply of 3.3v VDD. Can i connect…
Other Parts Discussed in Thread: SN6501 , SN6507 I'm looking for a way to implement a Transformer Driver into my design. The main issue here is the voltage and amperage requirements. The driver is meant to isolate a 57 V voltage rail and drive a current…
Part Number: UCC23313-Q1 Other Parts Discussed in Thread: CSD19536KTT , SN6501 , , TPSI3050-Q1 Dear TI team,
i am planning to design High side MOSFET driver for EV Battery pack with help of CSD19536KTT, UCC23313-Q1 & SN6501.
i want to get the block…
Hi Richard,
Thanks for your clarification.
If 90% Duty Cicle is accettable, do I need yet the SN6501 or SN6505 or the Full H-Bridge can work without them?
i.e. if the scenario is the following:
The motor always runs in the same direction with…
Hi Rao,
You may have right:
the problem is should not caused by the isolator (since no HV signal between the two grounds): When I touch with a piece of wire the Power transformer secunder winding or one of SPI (especially SCK) signals the noise dramatically…
Part Number: UCC27712 Other Parts Discussed in Thread: UCC27288 , UCC27624 , SN6501 Hi,
I am designing a charger for a LiFePO4 battery and need to switch just a high-side FET.
I decided to use the UCC27712
My question is, can I use just the high…
Hello,
It sounds like the main issue is to address the floating high side driver bias and the limitations of the bootstrap diode method for generating the high side bias.
This bias approach is limited regarding long on times or DC operation of the…
Part Number: AMC131M03 Other Parts Discussed in Thread: ADS131M04 , , SN74LVC1G17 , AMC3336 , AMC1336 , AMC0386 , SN6501 , UCC33020 , ADS1204 , ISO6761 Tool/software:
Hi im using AMC131M03 and ADS131M04, im having an issue in crc, in what are the ways…