Part Number: SN6505A Hi TI team,
We use SN6505A to make a isolation power.
There are some abnormal boards showed the power supply is restarted in cycle.
The board works normally at the beginning and after several hours when the temperature is high(Actually…
Part Number: SN6505A Hi team,
Can I know the internal pull-down resistance of EN pin? My customer wants to pull-up the EN pin and wants to know what's the best pull-up resistance.
Regards,
Xiaoying
Hi Dirk,
The UCC25800 is from a different product group but from looking at the datasheet the internal MOSFETs seem to be rated at 500mA RMS current as against the MOSFETs in SN6505A which are rated at 1A. I would also like to mention that UCC25800 isn…
Part Number: SN6505A Hi expert,
May I know what's the design consideration for the inductor of Voltage-uSecond spec? Is 40 must needed? What we typical see this parameter is 10~24.
Regards,
Allan
Part Number: SN6505A-Q1 For the figures entitled "Efficiency vs Load Current" (for example Figure 6-2), does the efficiency estimate include the losses from the diode?
Part Number: SN6505A Other Parts Discussed in Thread: SN6507 Hi Team:
My customer want to use SN6505A to make a 6W power module as 5V/1.2A.
But i check the spec of ILIM is more than 1.2A. so would you help to check whether we can reach to 1.2A ? and why…
Hi JC,
They tried the method you commented, but they could not find the SN6505A. Could you please let me know if there are any points to note?
Thank you for your help.
Regards,
Taito Takemura
Part Number: SN6505A Other Parts Discussed in Thread: PMP4190 , , , SN6505B , TINA-TI I have design Low wattage SMPS using of SN6505A and PMP4190.
Input-5V(3 to 6)
Output- 5V/400mA
Isolation-1500VDC
Please share me reference Design as above part number. …
Part Number: SN6505A-Q1 Hi,
I am using the SN6505AQDBVTQ1 for an automotive DCDC but it is impossible to get any sample.
Have you got a solution?
Best regards
Yoann
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A , SN6505B Hello,
I am having an issue with my design, as shown below. The voltage at Pin.2 of the transformer (750313769) is pulling P5V0 from 5V to less than 2V and back to 2V to 5V.
I want…