Hi Manoj,
Thanks for your inputs and sorry, yes the power consumption should be "I^2 * R", that was a silly mistake from my side. With the corrected calculations, the power loss or dissipation is going to be 123mW (instead of 61mW). The temperature difference…
Part Number: SN6505B Other Parts Discussed in Thread: SN6501 , Hello TI team,
I need to implement an isolated CAN Bus node based on the spec sheet recommended design of the transformer driver SN6501 or SN6505B.
Question 1
If not used, can pin 6 (CLK) of…
Part Number: SN6505B Hello TI-Support Team,
I have a problem with a push-pull-converter setup using SN6505B and Wuerth 760390012.
The SN6505B is provided with external clock (500 kHz) and enable signals. The circuit (see picture) is like the datasheet…
Part Number: SN6505B-Q1 Hi there,
In the component datasheet, all reference design are using same voltage for SN6505B-Q1 (VCC) and primary winding of transformer.
In my application i would like to have two different voltages, for:
…
Part Number: SN6505B This circuit generates a negative isolated 15V
At higher air temperatures >= 65°C the output skips operation - load is around 55mA average
What could be the issue here?
Part Number: SN6505B Other Parts Discussed in Thread: TPS7A05 , SN6505A Hi,
We have to power supply a 4 channels isolated data acquisition system and we are looking for an ultra low-power isolated DC-DC converter with the following specs:
VIN: from a 3…
Hello Vamsi,
I apologize for the confusion. I meant to show that I have provided the information to your questions regarding gate charge and rise and fall time in my initial reply, please review and follow up with additional questions or information here…